跳转到主内容
Knowledgebase
Home
Renesas Electronics China - Knowledgebase

Conditions of the HALT status is entered other than memory shortage

Latest Updated:12/01/2011

Question:

Control shifts to the initial block of the nucleus and the HALT status is entered.
Are there any conditions under which this will happen other than memory shortage?

Answer:

The OS enters the HALT status when a management table cannot be created for some reason, rather than due to memory shortage.
In addition, check to make sure there is no program lockup or memory error.
Suitable Products
  • 这篇文章对您有帮助吗?