跳转到主内容
Knowledgebase
Home
Renesas Electronics China - Knowledgebase

What is AQL (Acceptable Quality Level)?

Latest Updated:08/01/2005

Question:

AQL (Acceptable Quality Level)

Answer:

Indicates the minimum quality value (upper-limit failure rate) at which sampling inspection is aggressively judged to be acceptable.



For details, refer to the Review of Quality and Reliability Handbook.
Suitable Products
  • 这篇文章对您有帮助吗?