跳转到主内容
Knowledgebase
Home
Renesas Electronics China - Knowledgebase

Is the life of semiconductor devices affected by temperature?

Latest Updated:04/01/2009

Question:

Is the life of semiconductor devices affected by temperature?

Answer:

Yes. Temperature and degradation of electrical characteristics are closely related.
Generally, degradation accelerates as the temperature rises.
A semiconductor device rapidly degrades at temperatures that exceed the maximum rated temperature.
Care must be exercised when using devices at high temperatures.

Reference document:
Review of Quality and Reliability Handbook
Suitable Products
 
  • 这篇文章对您有帮助吗?