跳转到主内容
Knowledgebase
Home
Renesas Electronics China - Knowledgebase

Received Signal Strength Indicator (RSSI) value of Peripheral

Last Updated:09/20/2017

Question:

Can the RL78/G1D acquire the value of the Received Signal Strength Indicator (RSSI) of the remote device?

Answer:

Yes, the RSSI values can be obtained either before or after connecting to the peripheral devices in the following ways.

Before connecting, there are two ways to obtain the RSSI value of the peripheral device:

1.    Call the RBLE_GAP_Observation_Enable function to execute the scan and obtain it from the advertising report notification event RBLE_GAP_EVENT_ADVERTISING_REPORT_IND.
2.    Call the RBLE_GAP_Device_Search function to execute the scan and obtain from the device search result notification event RBLE_GAP_EVENT_DEVICE_SEARCH_RESULT_IND.

After connecting, you can obtain the RSSI value of the designation remote device by doing the following:

1.    Call the RBLE_GAP_Read_RSSI function to acquire from the RSSI acquisition completion event RBLE_GAP_EVENT_READ_RSSI_COMP.

For details of each function and event, refer to the following manual.

Bluetooth® Low Energy Protocol Stack API Reference Manual: Basics (R01UW0088)
https://www.renesas.com/search/keyword-search.html#q=R01UW0088&genre=document

Suitable Products
RL78/G1D
Bluetooth
  • 这篇文章对您有帮助吗?