跳转到主内容
Knowledgebase
Home
Renesas Electronics China - Knowledgebase

Connecting to Remote Device Registered in White List

Last Updated:09/20/2017

Question:

How can I connect to a remote device registered in the White List?

Answer:

Register the Bluetooth Device Address (BD_ADDR) in the White List when pairing. By calling the RBLE_GAP_Create_Connection function with the RBLE_GAP_INIT_FILT_USE_WLST set to init_filt_policy parameter, only devices registered in the White List will be connected.

For details, refer to the following manual:

Bluetooth® Low Energy Protocol Stack API Reference Manual: Basics (R01UW0088)
https://www.renesas.com/search/keyword-search.html#q=R01UW0088&genre=document

Suitable Products
RL78/G1D
Bluetooth