跳转到主内容
Knowledgebase
Home
Renesas Electronics China - Knowledgebase

Lowest current consumption configuration

Last Updated:02/13/2017

Question:

What RL78/G1D configuration has the lowest current consumption?

Answer:

Current consumption is lowest when using built-in DC-DC and external slow clock are selected.
Suitable Products
RL78 Family
RL78/G1D
Connectivity
Bluetooth