跳转到主内容
Knowledgebase
Home
Renesas Electronics China - Knowledgebase

Bluetooth SIG Qualification of RL78/G1D module based products

Last Updated:02/13/2017

Question:

Do RL78/G1D module (RY7011A0000DZ00) based products need Bluetooth SIG Qualification? 

Answer:

Registration of the "End Product" is required. RL78/G1D module (RY7011A0000DZ00) based products may be added to QD ID (82194) belonging to RY7011A0000DZ00.  A Declaration ID Fee (8,000 USD for adopter members) is needed for registration.

Listing Details for the RL78/G1D module (RY7011A0000DZ00) can be available at: 
     https://www.bluetooth.org/tpg/QLI_viewQDL.cfm?qid=30329

Suitable Products
RL78/G1D
Bluetooth