跳转到主内容
Knowledgebase
Home
Renesas Electronics China - Knowledgebase

How can I update my compilers with e2 studio update program?

Latest Updated:11/21/2016

Question:

I want to install compilers. And can I update my compilers with e2 studio update program?

Answer:

Compiler products are not included in e2 studio. e2 studio can update the plugin of eclipse but cannot update external programs like compilers.
Please download compilers you need from the pages listed below and install them.


[Compiler Products Sites]
For Renesas Compiler Products, visit here.

For GNU Tools compilers, visit here.

Note: Free user registration is required to download these compiler products.

Suitable Products
e² studio