跳转到主内容
Knowledgebase
Home
Renesas Electronics China - Knowledgebase

How can I add variables to the Variables view?

Latest Updated:12/09/2014

Question:

How can I add variables to the Variables view?

Answer:

"The Variables view shows local variables of  a function which is running on debugger.
Please add desired variables to the Expressions view and see the variables on the view."
Suitable Products
e² studio