跳转到主内容
Knowledgebase
Home
Renesas Electronics China - Knowledgebase

Why is the code preview not available in the [Project Tree] panel?

Latest Updated:03/11/2015

Question:

Why is the code preview not available in the [Project Tree] panel?

Answer:

When you are using any of the MCUs given below, the code preview is not available in the [Project Tree] panel.
V850, 78K0, 78K0R, RL78/G12, RL78/G13, RL78/G14, RL78/G1A, RL78/I1A, RL78/L12, RL78/F12, RL78/F14

To view the source code, follow the procedure below to open the [Code Preview] panel.
While some of the descriptions may differ from those given in the CS+ Code Generator Tool Integrated Development Environment User's Manual: Peripheral Function Operation [CS+ for CC][CS+ for CA,CX], there are no differences in functionality.

1. Choose [Code Generator Preview] from the [View] menu.

2.The [Code Generator Preview] panel will open.

Suitable Products
CS+ (formerly CubeSuite+)