跳转到主内容
Knowledgebase
Home
Renesas Electronics China - Knowledgebase

Using a project built on CS+ on another family device

Last Updated:05/31/2017

Question:

How can I use a project which was built on CS+ as a CS+ project on another family device?

Answer:

To use the project on another family device;

When creating a new project, select the [Pass the file composition of an existing project to the new project] check box in the [Create Project] dialog box, and select an existing project and create a new project.

See here for details.

Suitable Products
CS+ (formerly CubeSuite+)
  • 这篇文章对您有帮助吗?