跳转到主内容
Knowledgebase
Home
Renesas Electronics China - Knowledgebase

Saving information collectively (CS+)

Last Updated:05/17/2017

Question:

I am using the CS+ for CC Integrated Development Environment. Although I can display various information such as a list of functions and transition graphs, is it possible to save all the information collectively?

Answer:

Use the Smart Report for the CS+ for CC Integrated Development Environment.

It allows you to collectively output various information such as a list of program sources, build option settings, information about functions and variables, and coverage ratio.

To start the Smart Report, select [Output Data for Quality Records Collectively...] in the [Project] menu of CS+ for CC.

This function is available in CS+ for CC V4.01.00 and later.

Click here for details of the Smart Report.

Suitable Products
CS+ (formerly CubeSuite+)
  • 这篇文章对您有帮助吗?