跳转到主内容
Knowledgebase
Home
Renesas Electronics China - Knowledgebase

Editor opened at every break (CS+ Integrated Development Environment)

Last Updated:06/07/2017

Question:

I am using the CS+ integrated development environment.

When I break program execution during debugging, the source file at the break point is opened by the editor. When I repeat this operation, source files are opened at every break. Is it possible to specify the settings so as to switch display on one editor screen?

Answer:

You can display source files without adding editor panels at every break by using the window recycling of CS+.

Window recycling is disabled by default. To enable this function, select the [General - Text Editor] category in the Option dialog box, and then select the [Use window recycling] check box.

For details about the [General - Text Editor] category in the Option dialog box, see this site.

Suitable Products
CS+ (formerly CubeSuite+)