跳转到主内容
Knowledgebase
Home
Renesas Electronics China - Knowledgebase

E2000002 Error Opening File after Windows Update_CS+

Last Updated:01/31/2018

Question:

When double-clicking on the source file to open it on the CS+ project tree after Windows update, I got the following error and cannot open the file.

Error (E2000002): Error opening file

[Direct Error Cause]
No FontFamily element found in FontFamilyCollection that matches current OS or greater: Windows7SP1

How do I resolve this?
 

Answer:

The error occurred because of the Windows Update.

Refer to the Microsoft web page at the URL below to resolve it.

"TypeInitializationException" or "FileFormatException" error in WPF applications that request fallback fonts after you install the January 9, 2018, .NET Security and Quality Rollup (KB4055002)

Further updates may be posted to the above page, so please check it regularly for latest information.

You can edit the source file with an external editor and perform work such as building and debugging with the CS+.

Suitable Products
CS+ (formerly CubeSuite+)
  • 这篇文章对您有帮助吗?