跳转到主内容
Knowledgebase
Home
Renesas Electronics China - Knowledgebase

Display of included files (CS+ Integrated Development Environment)

Last Updated:06/07/2017

Question:

I am using the CS+ integrated development environment.

On the project tree, registered source files are displayed. How can I display files included by source files?

Answer:

CS+ has a function to display dependency files. This function is disabled by default.

To enable this function, select the [General - Build] category in the Option dialog box, and then select the [Show dependency files in project tree] check box.

For details about the [General - Build] category in the Option dialog box, see this site.

Suitable Products
CS+ (formerly CubeSuite+)