跳转到主内容
Knowledgebase
Home
Renesas Electronics China - Knowledgebase

Confirmation of a variable write during a specific interval (CS+)

Last Updated:05/17/2017

Question:

I am using the CS+ for CC Integrated Development Environment. Can I check the variable written during a specific interval?

Answer:

Use the exclusive control check tool for the CS+ for CC Integrated Development Environment. (RH850 family only)

The tool allows you to easily check if you have changed a variable during a specific interval (e.g., interrupt enabled interval). This allows you to check if exclusive control is being performed normally.

For how to start this tool, open the Solution List panel in CS+ for CC and roll the mouse cursor over the exclusive control checker icon. The details will be shown on the right.

This tool is available in CS+ for CC V4.00.00 and later.

Click here for details of Exclusive control checking tool.

Suitable Products
CS+ (formerly CubeSuite+)
  • 这篇文章对您有帮助吗?