跳转到主内容
Knowledgebase
Home
Renesas Electronics China - Knowledgebase

Why are Task trace window and task analyze window not displayed?

Latest Updated:12/07/2009

Question:

Task trace window and task analyze window are not displayed.

Answer:

E8a emulator does not support task trace window and task analyze window. Also if you use E10A-USB emulator with a cable for 14 pins connector, task trace window and task analyze window are not displayed.
You can display task trace window when using a cable for 36 or 38 pins cable.
Suitable Products
High-performance Embedded Workshop
E10A-USB
HI7750/4 Real-time OS for SuperH Family
HI7700/4 Real-time OS for SuperH Family
HI7000/4 Real-time OS for SuperH Family
HI1000/4 Real-time OS for H8SX, H8S Family
High-performance Embedded Workshop Real-Time OS Aware Debugging