跳转到主内容
Knowledgebase
Home
Renesas Electronics China - Knowledgebase

What performance do the standard library functions have ?

Latest Updated:10/28/2014

Question:

What performance do the standard library functions have ?

Answer:

The size and performance in execution of the standard libraries is easily measured by using the simulator that comes with the compiler.
If you do not already have the product, download the free evaluation version of the compiler to check the performance of the libraries.
Suitable Products
CS+ (formerly CubeSuite+)
High-performance Embedded Workshop