跳转到主内容
Knowledgebase
Home
Renesas Electronics China - Knowledgebase

What does the functions generated by high-performance HEW means?

Latest Updated:09/10/2007

Question:

[High-performance Embedded Workshop V.4]  I do not understand the meaning of functions automatically generated by high-performance Embedded Workshop.

Answer:

Please refer to our application notes. It is described in chapter2.

Select a product from the following, and enter the Document No. to a search field of our website. The search field is in the upper-right corner of the screen.

  • C/C++ Compiler Package for SuperH RISC engine family 
    • Document No. REJ05B0463-0200
  • C/C++ Compiler Package for H8SX,H8S and H8 families
    • Document No. REJ05B0464-0200
  • C Compiler Package for M16C families
    • Document No. REJ10J0820-0100Z
Suitable Products
High-performance Embedded Workshop