跳转到主内容
Knowledgebase
Home
Renesas Electronics China - Knowledgebase

Target CPU not displayed on the CPU selection screen in Step 1

Latest Updated:05/06/2011

Question:

[High-performance Embedded Workshop V.4, V.3, V.2] I am trying to create a new project, but the target CPU is not displayed on the CPU selection screen in Step 1. In this case, how can I create the project?

Answer:

Some new devices are not listed in the CPU selection list in the Create Project window of the High-performance Embedded Workshop. In this case, please try the following procedure.

  1. Download and install the latest revision update for your compiler package.
  2. If the CPU you are using is still not listed after the update, use the Device File Updater which can add the CPUs to the CPU selection list.
    For details about the added CPUs, please refer to the Product Versions and The Added CPU Types from here.
  3. If you cannot apply both of the method in Section 1 and 2, use one of the following methods.
     
    1. When creating a new project, select the corresponding Family as the "CPU Series" in the CPU Selection window (Step 1), then select the CPU that is most similar to the CPU development project as the "CPU Type".
      Modify the device information (I/O definition file, vector table, etc.) in the automatically created files using the hardware manual as a reference.
    2. When creating a new project, select the corresponding Family as the "CPU Series" in the CPU Selection window (Step 1), then select "Other as the "CPU Type" and start to create the project. When building a project by selecting "Other," files that are dependant on device information are only created as templates. Use the hardware manual as a reference to add the necessary information.

Note that the files automatically created in the High-performance Embedded Workshop are sample files only. Although the descriptive contents of each file have been carefully confirmed, the user should always thoroughly validate the contents before embedding in a product.

Suitable Products
High-performance Embedded Workshop
C/C++ Compiler Package for SuperH Family
C/C++ Compiler Package for M16C Series and R8C Family [M3T-NC30WA]
C Compiler Package for R32C Series
C/C++ Compiler Package for H8SX, H8S, H8 Family