跳转到主内容
Knowledgebase
Home
Renesas Electronics China - Knowledgebase

Can you tell me functions of CPU supported by simulator?

Latest Updated:09/10/2007

Question:

Can you tell me functions of CPU supported by simulator?

Answer:

The supported functions depend on CPU series. Please refer to Chapter2.3 Simulation Range in Simulator/Debugger Part of High-performance Embedded Workshop User’s Manual.
Suitable Products
High-performance Embedded Workshop
C/C++ Compiler Package for SuperH Family
C/C++ Compiler Package for H8SX, H8S, H8 Family