跳转到主内容
Knowledgebase
Home
Renesas Electronics China - Knowledgebase

Is the FDT complies with both English and Japanese operating systems?

Latest Updated:06/04/2004

Question:

[Flash Development Toolkit V.2, V.3, V4] Is the Flash Development Toolkit compliant with both English and Japanese operating systems?

Answer:

Yes, it is.
Suitable Products
Flash Development Toolkit