跳转到主内容
Knowledgebase
Home
Renesas Electronics China - Knowledgebase

Is it possible to combine more than two files?

Latest Updated:06/04/2004

Question:

[Flash Development Toolkit V.2, V.3, V.4] Is it possible to combine more than two files?

Answer:

Yes, it is. Please register more than two files on the Target files, then combine them together by using [Build Device Image] function.
Suitable Products
Flash Development Toolkit