跳转到主内容
Knowledgebase
Home
Renesas Electronics China - Knowledgebase

How to know which microcomputer is compliant with FDT?

Latest Updated:05/14/2009

Question:

[Flash Development Toolkit V.2, V.3, V.4] How can I know which microcomputer is compliant with which Flash Development Toolkit?

Answer:

For the target devices of V.4, please refer to here.

For the target devices of V.3 and V.2, please see the Information about the previous version on our web page from here.
Suitable Products
Flash Development Toolkit