跳转到主内容
Knowledgebase
Home
Renesas Electronics China - Knowledgebase

What is the status of built in transistor on RESET before & after reset?

Latest Updated:07/04/2003

Question:

(Reset)   What is the operating status of the built-in pull-up transistor on the RESET pin before and after reset?

Answer:

The pull-up resistor is always on. (#105016)
Suitable Products
4508
4509
4559
455A
4571
  • 这篇文章对您有帮助吗?