跳转到主内容
Knowledgebase
Home
Renesas Electronics China - Knowledgebase

Is FFFFCh + FFFFDh + FFFFEh & FFFFFh used in ROM code protect control?

Latest Updated:03/08/2012

Question:

The ROM code protect control address (FFFFFh) overlaps with the reset vector address (FFFFCh to FFFFFh). Does this mean that the actual reset vector address is FFFFCh + FFFFDh + FFFFEh and the address FFFFFh is used for the ROM code protect control?

Answer:

Yes.
Regarding M32C/80 and M16C/80 Series, the ROM code protect control address is "FFFFFFh" and the reset vector address is "FFFFFCh to FFFFFFh".

Suitable Products
M32C/88
M32C/87
M32C/85
M32C/84
M32C/83
M32C/80
M16C/62A
M16C/62A(M16C/62T)
M16C/62M
M16C/62N
M16C/62N(M3062GF8NFP, M3062GF8NGP)
M16C/62P
M16C/6N4, M16C/6N5
M16C/6NK, M16C/6NL, M16C/6NM, M16C/6NN
M16C/30P
M16C/29
M16C/28
M16C/26A