跳转到主内容
Knowledgebase
Home
Renesas Electronics China - Knowledgebase

Causes of variety: Accuracy & precision of low on-chip oscillator?

Latest Updated:02/09/2009

Question:

What causes variation in the accuracy and precision of the low-speed on-chip oscillator?

Answer:

General causes of variation are:

  • Manufacturing variation (chip variation)
  • Variation caused by supply voltage fluctuation
  • Variation caused by ambient temperature
Suitable Products
R8C/1x
R8C/2x
R8C/3x
R8C/Lx
R8C/Mx