跳转到主内容
Knowledgebase
Home
Renesas Electronics China - Knowledgebase

Can I reprogram on-chip Flash rewrite mode & execute control program

Latest Updated:03/22/2012

Question:

Can I reprogram on-chip Flash in the CPU rewrite mode while executing the control program in the boot ROM or user ROM area?

Answer:

It is possible if EW1 mode is used. In EW1 mode, the reprogramming control program in the on-chip ROM area can be executed and the on-chip flash memory can be reprogrammed.
However, the block that contains the reprogramming control program is excluded from the reprogramming.
Suitable Products
M32C/83
M16C/62A(M16C/62T)
M16C/62M
M16C/62N(M3062GF8NFP, M3062GF8NGP)
M16C/62P
M16C/63
M16C/64
M16C/64A
M16C/64C
M16C/65
M16C/65C
M16C/6C
M16C/6N4, M16C/6N5
M16C/6NK, M16C/6NL, M16C/6NM, M16C/6NN
M16C/5L, M16C/56
M16C/5LD, M16C/56D
M16C/5M, M16C/57
M16C/30P
M16C/29
M16C/28
M16C/26A