跳转到主内容
Knowledgebase
Home
Renesas Electronics China - Knowledgebase

Can driving of a 3 terminal regulator increase by parallel connection?

Latest Updated:12/01/2011

Question:

Can the driving current of a 3-terminal regulator be increased by parallel connection?

Answer:

No.
If the current is insufficient, dissipates the heat or connect a transistor to the output.
Reference:Usage of Three-Terminal Regulators
Suitable Products
3 Terminal Regulators