Can I use the UPD5200, 5201, or 5205 with a single power supply?
Latest Updated:09/01/2007
Question:
Can I use the UPD5200, 5201, or 5205 with a single power supply?
Answer:
Each of uPD5200, uPD5201, and uPD5205 is specified for use with a dual power supply, so you must not use it with a single power supply. Use it under the recommended conditions listed in the Data Sheet.
Suitable Products