跳转到主内容
Knowledgebase
Home
Renesas Electronics China - Knowledgebase

How do the numbers end in -00 and -E0 differs in the part of RJK5012DPP?

Latest Updated:09/02/2013

Question:

The RJK5012DPP has orderable part numbers ending in -00 and -E0. The outer dimensions look slightly different. Are the electrical characteristics the same?

Answer:

Both of the below RJK5012DPP products have the same electrical characteristics and both have a TO-220 insulated package. The outer dimensions are different.

  • E0: TO-220FP
  • 00: TO-220FN (Not recommended product)
Suitable Products
Power MOSFETs for General Switching