跳转到主内容
Knowledgebase
Home
Renesas Electronics China - Knowledgebase

Explanation of Transistor orderable part numbers

Latest Updated:10/05/2016

Question:

What is the difference between each part number?

Answer:

Please refer to the links in the below table which link to the appropriate page in the "explanation of orderable part numbers" document.

Please note that this table includes products regardless of status (mass production, non-promotion, others).

Suitable Products
Transistor
  • 这篇文章对您有帮助吗?