跳转到主内容
Knowledgebase
Home
Renesas Electronics China - Knowledgebase

Can you differentiate the 2SK1522-E and 2SK1522-E1-E and what is E1?

Latest Updated:09/02/2013

Question:

What is the difference between the 2SK1522-E and the 2SK1522-E1-E? What does "E1" mean?

Answer:

The difference between the 2SK1522-E and the 2SK1522-E1-E is a "Package Change" due to a change in assembly plant. TO-3PL has changed to TO-264.
Suitable Products
Power MOSFETs for General Switching