跳转到主内容
Knowledgebase
Home
Renesas Electronics China - Knowledgebase

Any alternatives/same product with similar specs to 2SK3225?

Latest Updated:09/02/2013

Question:

Is there any substitute/equivalent product with similar specs to the 2SK3225? It doesn't matter if the package is different.

Answer:

For the 2SK3225 (lead type), the RJK0631JPD is a substitute/equivalent product, although it has a different package shape.
Suitable Products
Power MOSFETs for General Switching