跳转到主内容
Knowledgebase
Home
Renesas Electronics China - Knowledgebase

What extent (volts) is the surge suppressed?

Latest Updated:11/01/2005

Question:

If a static electricity of 8 kV is applied to surge protection diode NNCD5.6LH, to what extent (volts) is the surge suppressed?

Answer:

According to the result of a test with the IEC61000-4-2, the diode clips at around 2.5 kV when 8 kV is applied.
Suitable Products