跳转到主内容
Knowledgebase
Home
Renesas Electronics China - Knowledgebase

Are there dimensional drawings of endorsed mount pad for each product?

Latest Updated:09/02/2013

Question:

Are there any dimensional drawings of the recommended mount pad for each product?

Answer:

The recommended mount pad for each product is shown on its product information page.
Example: RJK0305DPB
Refer to the Package section of the below page.

*Reference information here
*The recommended mount pad for some products is shown under Package.

Suitable Products
Power MOSFETs for General Switching