跳转到主内容
Knowledgebase
Home
Renesas Electronics China - Knowledgebase

What is the maximum turn off time if the typical value is 250 ns for the 2SK1671?

Latest Updated:09/02/2013

Question:

The 2SK1671 datasheet shows the turn-off time as 250 ns (TYP). What is the maximum value?

Answer:

We have not specified minimum and maximum values for switching characteristics such as turn-off time for the 2SK1671. We generally specify Typ values for switching characteristics. Thank you for your understanding.
Suitable Products
Power MOSFETs for General Switching