跳转到主内容
Knowledgebase
Home
Renesas Electronics China - Knowledgebase

What are the avalanche energy (EAS, EAR) and current (IAP) of 2SK2723?

Latest Updated:09/02/2013

Question:

What are the avalanche energy (EAS, EAR) and avalanche current (IAP) of a MOSFET (2SK2723)?

Answer:

Avalanche energy (EAS, EAR) and avalanche current (IAP) are not specified for the 2SK2723. Please do not use this device in a range where avalanche operation could occur.

This article is written based on not recommended products.

Suitable Products
Power MOSFETs for General Switching