跳转到主内容
Knowledgebase
Home
Renesas Electronics China - Knowledgebase

In what conditions does 3-terminal regulator deactivated?

Latest Updated:02/01/2007

Question:

In what conditions is the overheat protection circuit of a 3-terminal regulator deactivated?

Answer:

It is automatically deactivated when the junction temperature (Tj) drops below the overheat protection circuit operating temperature (150 to 200°C) .
Suitable Products
CMOS Operational Amplifiers
Bipolar Operational Amplifiers
3 Terminal Regulators