跳转到主内容
Knowledgebase
Home
Renesas Electronics China - Knowledgebase

How much is the reverse recovery time (trr) of the RJK60S5DPK-M0?

Latest Updated:09/02/2013

Question:

How much is the reverse recovery time (trr) of the RJK60S5DPK-M0?

Answer:

Reverse recovery time trr is specified as "Body-drain diode reverse recovery time [trr]" in the datasheet, which is 400 ns Typ.

This article is written based on not recommended products.

Suitable Products
Power MOSFETs for General Switching