跳转到主内容
Knowledgebase
Home
Renesas Electronics China - Knowledgebase

Are there 3 terminal regulator of low that can output negative voltage?

Latest Updated:12/01/2011

Question:

Is there a 3-terminal regulator of low-dropout type that can output a negative voltage available?

Answer:

Unfortunately, no.
Supplement: The uPC79 Series and the uPC337 can produce a negative output voltage.
Suitable Products
Power Management Linear