跳转到主内容
Knowledgebase
Home
Renesas Electronics China - Knowledgebase

What kind of characteristic is the slew rate?

Latest Updated:12/01/2011

Question:

What kind of characteristic is the slew rate?

Answer:

The slew rate (SR) defines the pulse input response. It is a value of the output response of a voltage follower circuit (gain = 1) measured as the voltage amplitude per 1 us. The higher this value is, the faster the performance of the operational amplifier.

Suitable Products
Operational Amplifiers