跳转到主内容
Knowledgebase
Home
Renesas Electronics China - Knowledgebase

What is a single-power-supply operational amplifier?

Latest Updated:12/01/2011

Question:

What is a single-power-supply operational amplifier?

Answer:

This is an operational amplifier in which the GND level can be input when a single power supply is used. In other words, V- is included in the common mode input voltage range.

Suitable Products
Operational Amplifiers
  • 这篇文章对您有帮助吗?