跳转到主内容
Knowledgebase
Home
Renesas Electronics China - Knowledgebase

What happens if Zener diodes connect in parallel?

Latest Updated:08/01/2005

Question:

I would like to connect several Zener diodes in parallel to achieve loss dispersion, but can this be done without problems?

Answer:

Do not connect Zener diodes in parallel.
If several Zener diodes are connected in parallel and a voltage that exceeds the Zener voltage is applied, the Zener current becomes extremely unbalanced if there are even slight fluctuations in the Zener voltage, causing topical load concentrations In the case of combinations with large fluctuations in Zener voltage, sometimes only one of the Zener diodes switches on.
Suitable Products
 
  • 这篇文章对您有帮助吗?