跳转到主内容
Knowledgebase
Home
Renesas Electronics China - Knowledgebase

硬件手册中为了将E8a仿真器连到MCU,是否必须将与MCU的MODE引脚相连的上拉电阻器的值指定为4.7kΩ±10%?

最新更新:03/24/2009

Question:

在硬件手册中,为了将E8a仿真器连接到MCU,将与MCU的MODE引脚相连的上拉电阻器的值指定为4.7 kΩ ± 10%。能否使用其它阻值的上拉电阻?

Answer:

4.7 kΩ ± 10%的上拉电阻是根据E8a仿真器的内部电路和MCU的DC特性计算得到的获得“H”电平所需的值。如果采用其它阻值的上拉电阻,E8a仿真器将可能无法正常工作。
Suitable Products
R8C/1x
R8C/2x
R8C/3x
R8C/Lx
R8C/Mx
E8a