跳转到主内容
Knowledgebase
Home
Renesas Electronics China - Knowledgebase

What are "Communications Flags" in the uPD72042B Data Sheet ?

Latest Updated:02/01/2006

Question:

Section 6.1 in the uPD72042B Data Sheet contains a list of "Communication Flags". What are these?

Answer:

These are the communication flags (defined as arguments or global variables) used in the main and interrupt routines shown as a sample of microcomputer processing flows used to control the uPD72042B, which appear in chapter 6 of the data sheet. The flag names in the table are given by way of example only.
Suitable Products
  • 这篇文章对您有帮助吗?