跳转到主内容
Knowledgebase
Home
Renesas Electronics China - Knowledgebase

Types of MCU's Used for TPS-1 Host CPU

Last Updated:06/01/2017

Question:

Can only the V850 or other Renesas MCUs be used as the TPS-1's host CPU?

Answer:

TPS-1's parallel and serial interfaces to the host CPU are very generic. Therefore, almost any host CPU can be connected.
Suitable Products
TPS-1
  • 这篇文章对您有帮助吗?