跳转到主内容
Knowledgebase
Home
Renesas Electronics China - Knowledgebase

TSP-1 Stack PROFINET Certification

Last Updated:06/02/2017

Question:

Is the TSP-1 stack certified by PROFINET?

Answer:

The certification has to be done for each PROFINET device. The TPS-1 was certified the first time on the Phoenix Contact HMI board (by an external test lab) and therefore has a certified stack for this device according to Conformance Class C. But you need each new device to have its own certification, which can also be done at Phoenix Contact.
Suitable Products
TPS-1
  • 这篇文章对您有帮助吗?