跳转到主内容
Knowledgebase
Home
Renesas Electronics China - Knowledgebase

TSP-1 Fast Forward Support

Last Updated:06/01/2017

Question:

The TPS-1 has an IRT Bridge-Delay of <3µs. Does this mean that the TPS-1 supports fast forward?

Answer:

The Bridge Delay of <3µs indicates how quickly the frames pass through the switch. Fast forwarding is characterized by a shortened frame length. However, Fast Forwarding will be supported from the software release V1.1 onwards.
Suitable Products
TPS-1
  • 这篇文章对您有帮助吗?