跳转到主内容
Knowledgebase
Home
Renesas Electronics China - Knowledgebase

TPS-1 Transmission and Reception via FX Interface

Last Updated:06/01/2017

Question:

Does the TPS-1 possess the necessary firmware and hardware support for data transmission/reception via the FX interface?

Answer:

The hardware and software supports two FX interfaces. The required circuitry is described in the TPS-1 user's manual and a simple setting change with the TPS-1 Configurator is sufficient to use the FX interfaces.

 

Suitable Products
TPS-1
  • 这篇文章对您有帮助吗?